10/17/2017 5:33 PM | |
Joined: 7/2/2016 Last visit: 12/11/2023 Posts: 115 Rating: (29) |
Dear Import-User-1 as the number of IO exceeds the maximum for the S7-1200 family I recommend the S7-300 or S7-1500 (I have never used 1500 in my projects) but by the specifications it is great for medium / large applications (like yours), but it is important that you check other possible needs like: Redundancy, Safety applications, network protocols (PN / DP ...) and so you can choose the right model. Note: you should also consider whether IO will be used in the main rack or remote in the field, in which case the ET200S and ET200M family are good options. at TIA Selection Tool (online or donwnload) you can configure your rack and see the options/limitations very clear. below the link is a very good tool and you will have more benefits like complete bill of materials (MLFB) and check all accessories. lets try it... Best Regards, DINIZ --- if it was helpful please rate the post.
|
Last edited by: Diniz [7] at: 10/17/2017 5:36:32 PMhope this help, if it was helpful please rate the post! |
|
This contribution was helpful to1 thankful Users |
Follow us on