6/18/2018 4:58 PM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hello David, function with CPU 314-2 DP also, but I think is not free and is quite old Easy Motion Control V2.0 Now Available - Industry Support Siemens I think this is the new version v2.1: Easy Motion Control - Software for SIMATIC Controllers - Siemens and I'm sorry this software I have never used |
Last edited by: Ste39 at: 6/18/2018 5:01:04 PM |
|
This contribution was helpful to1 thankful Users |
6/19/2018 10:57 PM | |
Joined: 11/12/2017 Last visit: 2/27/2024 Posts: 174 Rating: (1) |
Guys, When creating a data block for the data storage of this 1 count module for ET200S I have a question: -For both the inputs and outputs bytes 0 - 3 and bytes 8 - 11, what data type do I need to create. Do I need to use a DINT (double integer)? -Can I also then just create the rest as bytes with standard 8 bits with BOOL data type? Thanks David. Attachment1 Count ET200S Parameters.pdf (205 Downloads) |
Follow us on