8/18/2018 9:35 AM | |
Posts: 1 Rating: (0) |
In NCU573.5 , while renishaw workpiece probe cycles are being executed ,they are stopping at particular block everytime and prompting error message. Triggering and inspection by renishaw is getting completed, but the measured values are not being copied by NC into work piece directory file called measuring results .L799 is the cycle for Deleting/writing measuring results into "Measuring results WPD". The NC particularly halting at block number N600 in L799.spf. and staying there forever.Its not going to next block number. Attached L799 spf here with. Kindly help us in resolving the issue. AttachmentL799.pdf (40 Downloads) |
Last edited by: nkknbs at: 8/18/2018 9:38:11 AM |
|
8/19/2018 5:22 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Hello, You should have post this query in SINUMERIK CNC automation systems product conference. Now in L799.spf program block N600 is written as "Stop request for - Wait until function has been acknowledge". So it is not inetruption. It is the sequence & this block is specifically added so that operator should confirm/acknowledge the steps carried out. HTH. |
Follow us on