7/27/2020 3:36 PM | |
Joined: 12/18/2014 Last visit: 4/23/2024 Posts: 32871 Rating: (4064)
|
At my knowledge, no. |
7/27/2020 4:10 PM | |
Posts: 31 Rating: (0) |
Okay, so is there a way to digitally download the LOGO! Soft Comfort software digitally? I can pay if required. |
7/27/2020 4:15 PM | |
Joined: 12/18/2014 Last visit: 4/23/2024 Posts: 32871 Rating: (4064)
|
A licensed full version? No. But you can buy the software online e.g. Amazon.
|
7/27/2020 4:26 PM | |
Joined: 12/18/2014 Last visit: 4/23/2024 Posts: 32871 Rating: (4064)
|
To my knowledge, the LOGO! sold without software, it has to be bought separately. |
7/27/2020 4:41 PM | |
Joined: 3/30/2020 Last visit: 4/23/2024 Posts: 4430 Rating: (925) |
Questions to try help on the topic -- @ixo65: Which files can he extract from the disk that would make it possible to install a upgrade? Alternative: |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
7/27/2020 4:49 PM | |
Posts: 31 Rating: (0) |
Yes I can, that's the next step I was planning to do. I have an external hard disk casing for 2.5" hard disks (which is basically a USB to SATA converter) which I use in such situations. I will be able to pull out the software, but I don't know if it's licenses is bound to the motherboard like Windows licenses are. |
Last edited by: Nitish_Patil at: 07/27/2020 16:49:54 |
|
7/27/2020 8:17 PM | |
Joined: 12/18/2014 Last visit: 4/23/2024 Posts: 32871 Rating: (4064)
|
I do not understand this question. If he has an official CD or DVD (which licenses his installation), he can upgrade. If it doesn't have an official CD or DVD, I wouldn't give any information even if I knew it. Then he should start a Support Request.
|
7/27/2020 8:50 PM | |
Joined: 3/30/2020 Last visit: 4/23/2024 Posts: 4430 Rating: (925) |
Hello. For Microwin (S7-1200) there exist an official FAQ to move licensed software. I hoped there is one for Logo! -- a legal way. |
Last edited by: qwazee at: 07/27/2020 21:22:16remove detailed description Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
Follow us on