6/8/2015 2:16 PM | |
Posts: 4 Rating: (0) |
Hello , thanks alot for your reply , I deal now with different BData componement installed on separate PCs , I installed BData application server on the first PC , the BData acquisition on the second PC and BData client on the third, my problem is I can't comunicate o the acquisition PC from the BData server . I added a hardware acquisition and I chosen the second PC "Acquisition PC" on the network then in wizard I have chosen PCS7/WinCC communication but when I load archive an error message appears "Cannot connect to host" although the PING command shows that there is a correct communication between the two PCs Please help me Thanks a lot ---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 6/8/2015 5:20:11 PMNew subject after splitting |
|
6/8/2015 5:21 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4775 Rating: (123) |
|
Follow us on