7/28/2020 5:04 PM | |
Joined: 7/7/2010 Last visit: 5/7/2024 Posts: 14688 Rating: (2351)
|
This may help: https://support.industry.siemens.com/tf//ww/en/posts/215-1al40-0xb0-hsp-file/219289 Unless that PLC has MB/TCP running by default (instead of profinet by default) or has PLC logic supporting MB/TCP, you should consider using S7 instructions GET/PUT and use native Siemens communications.
|
science guy |
|
7/29/2020 9:04 AM | |
Joined: 9/3/2008 Last visit: 5/8/2024 Posts: 921 Rating: (158) |
Any S7-1200 can use Modbus TCP. See FAQ 102020340 for an example. |
Michael |
|
8/1/2020 4:10 PM | |
Joined: 4/7/2015 Last visit: 11/23/2023 Posts: 27 Rating: (2) |
Hi, vinayakpara81292! You can find the relevant information in system manual of s7-1200(chapter 13). |
Last edited by: Jen_Moderator at: 08/03/2020 08:56:11Optimized link. |
|
8/1/2020 5:17 PM | |
Joined: 9/27/2006 Last visit: 5/8/2024 Posts: 12257 Rating: (2666) |
Hello vinayakpayab; You have already been given information from some of the best experts on S7-1200 PLCs in the forum. Your model, 6ES7215-1AL40-0XB0, is not part of the standard products of Siemens. Sometimes Siemens will modify an existing standard model to satisfy the requirements of a specific client, and give this "new" model a distinct part number, since the company it is designed for will have a minimum production contract covering a few years if it wants this particular modificatioon. This model number is not included in the Siemens Industry Mall, the electronic catalog Siemens uses to detail its automation equipment; see the screenshot below. If it cannot be found there, you will find no official description anywhere else in Siemens documents. In one of the first links in this discussion, mopS04 indicated that this was probably a 6ES7215-1AG40-0XB0 modified with additional RAM memory, and suggested that in your program you use this part number to insert the CPU in the hardware configuration. The 6ES7215-1AG40-0XB0 supports Modbus TCP functions MB_CLIENT and MB_SERVER, as all other CPUs of this family (as you can see from the system manual that was proposed earlier). I would suggest that you prepare a test project, using a S7-215-1AG40 as a target hardware, insert Modbus TCP functions in the test program and try to download to your CPU. If you have no problem downloading and the CPU goes onine, then you should proceed to your full program with confidence. Hope this helps, Daniel Chartier Edit: Look at the following link, from a Siemens reseller: https://www.plc-city.com/shop/en/siemens-simatic-s7-1200-cpu-1215c/6es7215-1al40-0xb0-nfs.html You will find a download link for the technical data sheet for the S7-215-1AL40 inside this webpage, but you might be disappointed in the lack of contents.... Compare it to the data sheet for the S7-215-1AG40, from the Siemens Support pages: https://support.industry.siemens.com/cs/pd/142915?pdti=td&dl=en&lc=en-WW D.C. |
Last edited by: dchartier at: 08/02/2020 11:43:44 |
|
This contribution was helpful to2 thankful Users |
Follow us on