12/7/2021 5:27 PM | |
Joined: 10/15/2007 Last visit: 7/17/2023 Posts: 46 Rating: (3) |
Hi Alan_B_Stard, with your provided information I believe none of the forum users will neither be able to provide help nor any ideas. Can you provide some more details about what exactly you mean with "upgrading a project"? Only upgrading your TIA project / SIMOCODE ES project from V15.1 to V17 or also e.g. CPU / device firmware versions? Can you also provide some more details about what exactly you mean with "The Scalance switch they are connected to show no connection."? Do you e.g. mean that the Ethernet-Link LED of corresponding Scalance switch - to which the SIMOCODE device is connected - is OFF? As your problem really sounds like a severe issue I would recommend to contact Siemens support directly: Kind regards |
12/9/2021 2:13 PM | |
Joined: 10/15/2007 Last visit: 7/17/2023 Posts: 46 Rating: (3) |
Hi, can you maybe upload a screenhot which shows the information "Scalance X208 diagnostics show nothing is connected on the SimoCode ports."? If Ethernet port LEDs "P" (green/yellow LEDs) of Scalance are OFF there is no ethernet connection/link to corresponding device. This would also explain, why PRONETA does not show corresponding devices. Additionally I would recommend to update your CPU 1515F-2 PN to a more recent firmware version: Firmware Update for CPU 1515F-2 PN You might also check if a newer firmware version for your Scalance X208 is available: SCALANCE X-200 managed |
Last edited by: LostMyMind at: 12/09/2021 14:16:29Last edited by: LostMyMind at: 12/10/2021 09:15:03 |
|
Follow us on