6/2/2021 9:34 AM | |
Joined: 3/26/2020 Last visit: 4/24/2024 Posts: 2 Rating: (0) |
Dear all, I have created a simple VB script in a faceplate trying to write a value in the only property that the faceplate has. I have used the key shortcut <CTRL + J> to access the property name, thus avoiding any typing errors. When I checked the syntax of the script in the faceplate, no error was found. But, when I tried to compile the project to start the simulation, the system encountered the following error: "The script ... contains an invalid tag reference". The version of TIA Portal that I have installed is 16 update 4. I leave you as an attachment the test project that I have created. Please, if anyone knows the solution to this problem, I would appreciate your answer. Thank you very much for your time.
AttachmentfpScriptTest.zip (416 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on