2/27/2015 3:39 PM | |
Joined: 8/3/2009 Last visit: 9/5/2025 Posts: 16343 Rating:
|
Hello cusco I think the following Link should help you. https://support.industry.siemens.com/cs/ww/en/view/101977510 Have a nice weekend Bye Murof ----- If the Information hepls, you could use the Rate Button |
Last edited by: Min_Moderator at: 3/4/2015 3:19:17 PMInsert link If this Information really helps, you could use the Rate function |
|
3/2/2015 9:25 AM | |
Posts: 1299 Rating:
|
Hello, with wincc v13 sp1 the problem is solved. if the panel has the version "13.0.1.0" you can use the smartserver with java version 8. K!ke |
3/2/2015 4:41 PM | |
Posts: 1 Rating:
|
Hello, did you read the link in Murofs answer? K!ke |
3/4/2015 3:13 PM | |
Posts: 1299 Rating:
|
Hello, I think the "Alternatives for Java V8" are working with Java V8 There is also described where you find the smartclient.exe K!ke |
6/29/2015 7:39 PM | |
Posts: 10 Rating:
|
Hello I do not speak English , Google translation.I had the same problem the solution is in the link siemens . But the most important part is that the windows 64 in the same installation folder path for java java 8 and 7 of the attached photo . x86, but not recognize that change java 8 Java7 greetings https://support.industry.siemens.com/cs/document/101977510?dti=0&lc=en-WW |
Last edited by: joseinfantas at: 6/29/2015 7:40:54 PMLast edited by: joseinfantas at: 6/29/2015 7:41:51 PMLast edited by: Min_Moderator at: 6/30/2015 2:14:44 PMChange formatting |
|
2/2/2016 9:42 AM | |
Joined: 2/2/2016 Last visit: 5/20/2025 Posts: 2 Rating:
|
Hi Murof, Yes, I update to v13.0.1.0, and 4 of my HMI (TP1500) works with IE. But, still 2 HMI will be blocked by JAVA 8. Do you have any suggestion? Thanks. |
Follow us on