3/27/2019 3:37 PM | |
Joined: 10/15/2007 Last visit: 7/17/2023 Posts: 46 Rating: (3) |
Hi ploktavo, assuming that you are using a 3RW52 Soft Starter together with 3RW5 communication module "PROFINET Standard (3RW5 980-0CS00)" According to Equipment Manual - SIRIUS 3RW5 PROFINET Communication module there are two data sources available: (1) cyclic process image input (PII) --> 16 bytes: (2) acyclic data record communication via SFB 52 ("RDREC"); kind regards |
This contribution was helpful to1 thankful Users |
Follow us on