5/2/2016 7:22 PM | |
Posts: 8946 Rating:
|
http://www.dummies.com/how-to/computers-software/ms-office/excel.html |
This contribution was helpful to
1 thankful Users |
5/4/2016 3:47 PM | |
Joined: 7/20/2006 Last visit: 6/11/2024 Posts: 128 Rating:
|
Hi Here you will find some example. https://support.industry.siemens.com/tf/ww/en/posts/use-of-source-file/3716/?page=0&pageSize=10 regards Edek |
This contribution was helpful to
1 thankful Users |
5/5/2016 11:07 AM | |
Joined: 9/23/2005 Last visit: 6/28/2024 Posts: 4590 Rating:
|
Automatic generation of an S7 data block with STEP 7 V5.x from an MS Excel 2003 table |
Regards, |
|
This contribution was helpful to
1 thankful Users |
5/18/2016 12:01 PM | |
Joined: 1/3/2006 Last visit: 2/19/2024 Posts: 726 Rating:
|
Hi Since you just need to sample to get yourself started so please find the attached excel file. This excel file creates the AWL file which I can then import into Step7. Please note that I made this file to prevent doing myself from repetitive task of calling same standard FB so many times. So basically this file just generate the awl of a FB which calls standard FB. Of course your standard FB may differ from what I have but again this is only as you mentioned for reference purpose. In this excel file just fill in the yellow columns and it will create the AWL file of that many conveyors in D drive. If you read the macro then you can see where you have to define the structure of the standard FB ;-) AttachmentFB3.zip (278 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on