12/14/2016 5:12 PM | |
Joined: 11/16/2015 Last visit: 7/12/2024 Posts: 8 Rating: (0) |
Hi Smiffy, I have a system of two PLC, S7-317PN/DP + CP343-1 and S7-416 + CP441-1 ISO please help me regarding ISO communication: 1. Can I use BSEND and BRCV if Iuse ISO transport connection? -> problem is that I cannot simulate PLC comunnication with AG_SEND annd AG_RECEIVE -> is there a way in PLCSIM to simulate ISO communication between two PLCs? 2. We have sucessfully simulated two PLCS S7-416 + CP441-1 over S7 connection (TCP/IP) -> PLCs are in multicomputing mode on same rack and TCP/IP communication is working in PLCSIM Best regards Nikola ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 12/15/2016 3:56:06 PMNew subject after splitting |
|
Follow us on