2/8/2011 10:51 AM | |
Joined: 4/14/2010 Last visit: 8/6/2024 Posts: 525 Rating:
|
[schnippschnapp] Dear Supporter I want to use the Simatic Wincc SCADA Software for Remote DATA Monitoring & Controlled Because it have Good Graphical arrangement & its Resolution. When i think for Wincc SCADA Software some Questions are Creating in my Mind. 1. Have the Wincc SCADA Software Compatibility with SIEMENS plc through Profibus or Ethernet TCP/IP..??? 2. Have the Wincc SCADA Software Accessibility for approximately 5,000 DATA Tags Monitoring.??? 3. How Much have the SCADA Software Accessibility About DATA acquisition and fast DATA logging.??? 4. How much SCADA Software have Resolution Effect and aspect Ratio for 37" LCD Display.??? 5. What is the SCADA software order Number and its Necessity Interface.??? 7= Which CPU have you Suggest for the processing of 5,000 Tags also have ability to connect with wincc SCADA Software through TCP/IP..???? Dear Sir You can suggest any other Hardware Software if required for above project which is already Discuss with you. Thanking you & assuring you of our fullest cooperation & prompt attention at all times. Regarded Muhammad Sarfraz Splitted from I want to the convert all protocol with profibus of all devices for Siemens S7-300 or 400 PLC |
Last edited by: O_Moderator at: 2/8/2011 11:20 AMnew subject after splitting MS |
|
2/8/2011 11:47 AM | |
Posts: 799 Rating:
|
Dear Muhammad Sarfraz, you will find an answer to all of your questions in the WinCC help with following link: WinCC: General information WinCC: Installation / Release Notes SIMATIC HMI WinCC V7.0 System description If you already got WinCC Install CD you can also use the WinCC Information System. Best regards (Bizur was a little faster |
Last edited by: efka at: 2/8/2011 11:48 AM |
|
Follow us on