8/3/2020 1:47 PM | |
Joined: 7/29/2013 Last visit: 4/19/2024 Posts: 52 Rating: (1) |
Hi, I´m facing a similar problem. I´m working whit a S7 1215C DC/DC/RLY firmware V3.0.2 and tia V16. Everything was fine until i decided to use two interruption blocks one hardware interruption type and other cycle interruption type (Set up: 250 ms) to execute GET function. After those changes the plc was trough warning flashing and do not recognize one di/do module associated. Maybe thinking a little one test i could do is reset to factory settings y try to download the project without interruption OBs. But what could be wrong whit what??? Here is the picture of the error ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 08/03/2020 14:19:46New subject after splitting |
|
8/3/2020 2:13 PM | |
Joined: 7/29/2013 Last visit: 4/19/2024 Posts: 52 Rating: (1) |
Hi, Done, here is the diagnostic file .txt Hope you can help me AttachmentDiagnostics.txt (102 Downloads) |
8/3/2020 3:07 PM | |
Joined: 7/29/2013 Last visit: 4/19/2024 Posts: 52 Rating: (1) |
Yes, I´m already done that several times and did not have succeed. Now i tried to make an empty project with the correct hardware config, download it but still in fails!!!
AttachmentDiagnostics_1.txt (101 Downloads) |
Follow us on