1/23/2020 10:57 AM | |
Joined: 9/30/2016 Last visit: 4/5/2024 Posts: 910 Rating: (6) |
Please also see the attached screenshots. We have a machine where the event texts for 2 of the Emergency Stops have been swapped. The CPU is CPU 315F-2 PN/DP and the flex panel is a TP177B. There is Alarm_S used. So the alarm texts are in the STEP 7 project. After a long search I found the involved texts in a library called "Alarm_1_DK" in a folder called "Text Libraries". The folder called "Text Libraries".is on the same level in the project as the folders "Sources" and Blocks". I have swapped the texts in "Alarm_1_DK" but I can't figure out how to download / implement the library to the PLC / flex panel. In another thread (https://support.industry.siemens.com/tf/ww/en/posts/where-do-i-modify-my-alarm-texts/226576/?page=0&pageSize=10) it was suggested that I could use "Options > AS-OS Connection Data > Transfer" but I don't see "AS-OS Connection Data" under "Options" even though I DO have AS-OS-Engineering installed. So how do I download / implement the library to the PLC / flex panel? AttachmentGH133C.zip (130 Downloads) |
1/29/2020 9:29 AM | |
Joined: 8/3/2009 Last visit: 4/25/2024 Posts: 12859 Rating: (1639)
|
Hello xmnj to implement Alarm_S alarms in the Panel, check out this FAQ: https://support.industry.siemens.com/cs/ww/en/view/24013249 Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
1/30/2020 10:51 AM | |
Joined: 9/30/2016 Last visit: 4/5/2024 Posts: 910 Rating: (6) |
Hello Murof, Thank you for answering. I have read your the contents in your link but as far as I can see it does not answer my question. I have a system where the alarms are already configured and working on the flax panel. The exception is that 2 alarm messages have been swapped. My question is: After swapping the 2 texts in "Alarm_1_DK" how do I download /implement this modified "Alarm_1_DK"? I have a hard time believing that such a small modification really requires that the whole alarm setup for the flex panel is made from scratch again - surely it must be possible to accomplish this in a simpler way?
|
Follow us on