2/5/2020 1:56 PM | |
Posts: 15 Rating: (1) |
Hello, On the board of the Mindconnect IOT2040 there are also connections (like for an Arduino Shield). Are they just for decoration or does any shield fit? Or is it a proprietary format? Best regards. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 02/06/2020 07:41:09New subject after splitting |
|
2/5/2020 2:30 PM | |
Joined: 12/12/2016 Last visit: 4/8/2024 Posts: 640 Rating: (60)
|
Hello, I spoke to a colleague from Mindsphere and he said you can actually connect one shield to the Mindconnect IOT2040. Check out page 88 in this manual. After onboarding the Mindconnect IoT you can select to read values from the I/O Shield. |
This contribution was helpful to1 thankful Users |
Follow us on