8/6/2020 1:42 PM | |
Joined: 3/2/2007 Last visit: 9/18/2024 Posts: 935 Rating: (5) |
Kindly, can we install motor modules at left side of Smart line module booksize (10kw or 16kw)? line modules 6SL3130-6AE21-0AB1 , 6SL31306AE210AB1| 6SL31306AE210AB1 , SINAMICS S120 SMART LINE MODULE INPUT: 3AC 380-480V, 50/60HZ OUTPUT: 600VDC, 17A, 10KW FRAME SIZE: BOOKSIZE INTERNAL AIR COOLING INCL. CONTROL VOLTAGE ADAPTER MODULES PAINTED 6SL3130-6TE21-6AA4 , 6SL31306TE216AA4| 6SL31306TE216AA4 , SINAMICS S120 SMART LINE MODULE INPUT: 3AC 380-480V, 50/60HZ OUTPUT: DC 600V, 27A, 16KW FRAME SIZE: BOOKSIZE INTERNAL AIR COOLING INCL. DRIVE-CLIQ CABLE https://mall.industry.siemens.com/mall/en/us/Catalog/Products/10314125 motor modules 6SL3120-2TE13-0AD0 , 6SL3120-2TE15-0AD0 , 6SL3120-2TE21-0AD0 , 6SL3120-2TE21-8AD0
|
... thank you ... |
|
8/6/2020 2:15 PM | |
Joined: 5/12/2006 Last visit: 9/24/2024 Posts: 22371 Rating: (3012)
|
yes why not. |
8/6/2020 8:22 PM | |
Joined: 5/22/2012 Last visit: 3/24/2022 Posts: 895 Rating: (67) |
... please check device Manual GH2. I Think for 5 and 10kW the Infeed must be on the left side. |
8/10/2020 11:05 PM | |
Joined: 10/12/2018 Last visit: 8/30/2022 Posts: 23 Rating: (1) |
Please see the attachment below from the s120 power component manual. Clearly states you can have the DC coupling on either side |
Follow us on