8/22/2020 10:40 PM | |
Joined: 7/31/2020 Last visit: 9/11/2024 Posts: 21 Rating: (5) |
Hello The smartview app is not more then a vnc client. it mirrors the HMI. so to answer your questions: 1:I want to use general pc station with plc 1200 not HMI is it correct or must use hmi? If you want to use the smartserver, you must use an HMI. Another option is to run the HMI on your PC using WinCC runtime advanced or create a user defined webpage for the PLC which is accessible from your PC (but this is a slow alternative and will require a lot of programming). I would advise you to look into wincc runtime advanced. https://new.siemens.com/global/en/products/automation/industry-software/automation-software/tia-portal/software/simatic-wincc-tia-portal/wincc-tia-portal-runtime-software.html you can always setup an vnc server on your PC and a vnc client on your phone to monitor the RT. 2:I want to use mobile network to do that not wi-fi how? you need to be in the same ip-range to access the hmi using the smartserver. it is possible over the mobile network but then you will need to configure a vpn. if you connect your phone as a vpn client it's possible to access the hmi. it's possible that siemens has out of the box solutions for this but i'm not aware of this, somebody else?? 3: hardware connection of network cables? there will always have to be a connection between the CPU and the visualisation (HMI or PC-Runtime) |
Last edited by: VeulemansJens at: 08/22/2020 22:44:16//Jens |
|
8/23/2020 8:06 AM | |
Joined: 2/12/2020 Last visit: 6/11/2024 Posts: 56 Rating: (1) |
Thanks alot for your replies. |
8/27/2020 3:30 PM | |
Joined: 2/12/2020 Last visit: 6/11/2024 Posts: 56 Rating: (1) |
concerning point no 2: 2:if i use astatic ip ,i can use amobile network thats ok or not? |
Follow us on