5/19/2020 8:52 AM | |
Posts: 1 Rating: (0) |
Hello,digiSUPport From ur description, I was wondering if the TIA 1500 could be replaced by S7-300 or 400. Is it because of the PLCSIM -advanced used in loop, so it must be corresponding with TIA1500, and PLCSIM to be corresponding with S7 300 or 400? I am on the structure forming stage, trying to do the MCD-SIMIT-S7 300 in pure software in loop, any advice for me? I would be appreciated. chen
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/19/2020 11:18:49New subject after splitting |
|