4/15/2016 11:08 AM | |
Posts: 5 Rating: (0) |
Hello, I have a problem using powerrate faceplates in Powerrate V3 in Wincc v7.0 I followed the powerrate configuration example for Powerrate V3, but when I click on PR3_SUM block icon the associated faceplates do not open as shown in the example . (the picture in attachment shows the part where you click and the associated faceplates open ) Also , I have put the picture I created under the container in picture tree manager and I configured it in OS project editor , nothing happened after running the runtime . Did I miss something? ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 4/15/2016 12:23:35 PMNew subject after splitting |
|