(1)| 7/2/2015 8:30 AM | |
|
Posts: 8 Rating:
|
Hello all, I am also facing the same problem other members are facing. I am new to SCADA WINCC OPC, I took the help of the PDF file supplied by SIEMENS which is "Communication WinCC - WinCC V6 Using OPC DA",In this PDF steps are explained to configure WINCC as OPC Server and as OPC Client(Refer Page 455 in PDF attached ). Now the problem I am facing is when I want to configure WINCC as OPC Client. In OPC Item Manager, when I select OPCServer.Wincc.1 under "LOCAL" network and Click "Browse Server", there is an error "could not access the selected OPC server". I have also made the necessary DCOM settings given in the PDF. I am also attaching the screen shots and PDF in rar file. Wincc installed: WinCC explorer V7.2 ---------------------------------------------------------------------------------------------------- Split from i can't find OPCServer.WinCC.
AttachmentOPC.rar (617 Downloads) |
Last edited by: Min_Moderator at: 7/2/2015 1:43:32 PMNew subject after splitting |
|
| 7/11/2015 3:48 PM | |
|
Posts: 8 Rating:
|
Thank you bg2492, you have solved my problem. Thank you very much. |
This contribution was helpful to
|
|
Follow us on