(0)| 7/14/2015 9:59 PM | |
|
Posts: 20 Rating:
|
I am having similar trouble with a 6SN1118-0aa11-0aa0 analog card with user friendly interface. Using a single axis 25A Power Module. SW9 on my Parameter board is only one that needs to be on according to table in the 611A function Guice. The motor i am trying to run is 1FT5072-1AF71-1AG0. I get a '7' on the 7-segment display when I enable the motor. 7 according to table means Speed controller at stop and Actual Current is 0. The motor is not connected to anything, so what is stopping it? I can run the power module with a Universal Control card to turn any motor.....the Power Module can''t be the problem. I was able to use a motor, 1FT5064-0AC71-2, and it ran good with the same card. Used the same feedback cable too. Don't think the cable is the problem. Is there something different between the motors that I am not seeing? The first zero in the second set means the motor is Standard Type. I am trying to figure out what makes my current motor, 1FT5072-1AF71-1AG0, not standard. Any thoughts? Anybody? Andy
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 7/15/2015 11:35:27 AMNew subject after splitting |
|
Follow us on