(2)| 9/17/2015 4:42 PM | |
|
Posts: 2 Rating:
|
Dear all, I face a problem of opening wincc project when I try to download my OS project from ES STATION, I have PCS7 v8.0 on my ES and OS,when I try to download os the process gets stop on the "opening wincc". 1-my users and their passwords are same on both systems, 2-all of the permissiones and and security of shared folder between both computers have been done based on Siemense instruction, Im looking forward hearing from you, mobin ------------------------------------------------------------------------------------------ |
Last edited by: CS Moderator at: 9/18/2015 9:44:17 AMNew subject after splitting |
|
| 9/18/2015 10:02 AM | |
|
Posts: 567 Rating:
|
Hello Mobin, there are a lot of reason why the download of the OS Project Fails. under the following FAQ you can find some Information what you can check if download not works. "What should you watch out for when downloading from the WinCC/PCS 7 Engineering Station to the Operator Station (ES-OS download)?" |
| 9/18/2015 6:18 PM | |
|
Posts: 2 Rating:
|
Hi dear, thanks for your response, |
| 8/25/2022 1:14 PM | |
|
Joined: 2/9/2014 Last visit: 3/18/2025 Posts: 16 Rating:
|
Hello nikola_hadjinikolov, I am also facing same issue and tried your remedy with no luck do you have any other solution? |
| 11/28/2024 6:50 AM | |
|
Joined: 12/20/2019 Last visit: 11/18/2025 Posts: 8 Rating:
|
It is mostly because of access rights. first Make sure of the same USER and PASSWORD and instead of giving the permissions manually to the shared OS folder on client, simply use the "SIMATIC RIGHTS" application which exists in PCS7 package usually in "Additional Products" folder. then share it. |
Follow us on