(0)| 12/8/2015 5:54 PM | |
|
Posts: 14 Rating:
|
Hi Christoph, My project is developed on ES with PDM V8.0 SP1 and mean while i edit the project in another PC with PDM V8.0 SP2. Now my problem is that i am not able to do any HW Config. changes, visible as readonly on ES with SP1.
Is there any way that i still could work on my project with SP1 ? without updating SP1 to SP2? - One more issue is that am able to do "Lifelist" but not able to upload, always error comes as "Object structure incomplete or damaged", checked EDD file is correct, In Other plant Area Project, same instrument works fine.
------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 12/9/2015 11:15:11 AMNew subject after splitting |
|
Follow us on