(0)| 2/13/2017 9:50 AM | |
|
Posts: 8 Rating:
|
------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 2/13/2017 10:14:04 AMNew subject after splitting |
|
| 2/13/2017 10:03 AM | |
|
Posts: 5521 Rating:
|
hi KyawHS, What Baud Rate is set in PB-master(CPU)? I guess 200-220m is to long for the actually set Baud-Rate. Set a lower Baud-Rate. Tha acceptabel line length of a PB-DP network you will find here: Acceptable line length in PROFIBUS-DP networks BF-LED is a Bus-Fault. So when the line-length is not the problem check the wiring and the termination resistors. hope this helps, regards, |
| 2/13/2017 5:49 PM | |
|
Posts: 623 Rating:
|
Hi KyawHS, U should connect profibus nodes one by one and not all nodes in single attempt. Also do not download PLC program and just download HW config. If u have followed this procedure and still problem persists then reduce baud rate. |
| 2/18/2017 9:08 AM | |
|
Joined: 4/25/2011 Last visit: 12/9/2025 Posts: 40 Rating:
|
Hi Friend, I hope this will help you. |
|
Nobody is Perfect and i am nobody....If it is helpful please Rate it. |
|
This contribution was helpful to
|
|
Follow us on