(1)| 1/29/2012 9:53 PM | |
|
Joined: 10/7/2005 Last visit: 12/29/2025 Posts: 3052 Rating:
|
Hello cy429 have a look at the the three Getting Started Guides below, they should contain all the answers for AI's that you are seeking: SIMATIC S7-300 SM331; AI 8x12 Bit Getting Started part 1: 4 -20mA SIMATIC S7-300 SM331;AI 8x12 Bit Getting Started Part 2: Voltage and PT100 SIMATIC S7-300 SM331; AI 8 x 12 Bit Getting Started part 3: Thermocouples Note too the small "Info" disk icon in the top right hand corner of each page which contains the download of the example program. Analogue Outputs are simply the "reverse" of AI's and the S7-300 Automation System Module Data manual is a must have referencefor both (see especially chapter 4, 5 & 6). The "TI to S7 converting library" contains ready made scaling blocks (FC105 and FC106) andyou'll find additonal info with a search on the subject at https://support.automation.siemens.com. I hope this helps |
|
Cheers |
|
This contribution was helpful to
|
|
| 2/5/2012 6:15 AM | |
|
Posts: 33 Rating:
|
thank you very much |
This contribution was helpful to
|
|
| 9/16/2013 2:34 PM | |
|
Posts: 24 Rating:
|
Im also looking for complete example,as requested. Complete means from the AI module receive the input signal ie 4-20mA, The signals then processed by AI module at PIWxx, scaled or unscaled,loaded to CPU, Transfered for PQWxx processing,sent to output module and displayed at TD200,or outputted as DzO to control on and off eqiipment. From what i read,most of the examples show only half of it,ie scaling alone,or PIW or PQW alone Without any extension to the next phase. Really realy apreciate if anybody have any example for S7 200 and 300.
Attachmentinfoplc_net_sitrain_13_analog_ processing.pdf (1944 Downloads) |
Last edited by: adamb at: 9/16/2013 2:41 PMLast edited by: adamb at: 9/16/2013 2:40 PMRefer attachment pg 2 Last edited by: adamb at: 9/16/2013 2:36 PM |
|
| 9/16/2013 9:28 PM | |
|
Joined: 1/28/2009 Last visit: 12/30/2025 Posts: 6891 Rating:
|
Hello, I can offer a humble sample for analog processing strategies in automation.You can find it here: FB41_EX.zipThere are other applications of analog signals such as alarm and trip generation based on level violation for protection issues and many others that you should encounter them in industry.You can search for other applications regarding functions FC105/FC106 that are discussed here. Best regards Hamid Hosseini |
This contribution was helpful to
|
|
| 1/22/2014 11:11 AM | |
|
Posts: 340 Rating:
|
new question is splittet to how use FC105 block to read PT100 RTD feedback value |
Follow us on