(0)| 8/14/2017 8:22 AM | |
|
Posts: 12 Rating:
|
Hi, fluidcontrol. Thanks for your reply. I have solved this problem almost as you recommended but some another way: In HMI Alarms took empty field, for example, "Additional text 1", and dublicate to this field value which in field "Alarm group". And in Alarm view -> Properties ->Alarm filter set filter to field "Additional text 1" in lieu of "Alarm group". It is a crutch but it works. There are once more issue that I can't resolve: I need to count number of alarms in different classes and groups. But I need to do it in script (C or VB doesn't matter) and start this script with some event or timer. I have considered functions which having in WinCC scripting but nothing till found. Can you some advice for this matter?
------------------------------------------------------------------------------------------ |
Last edited by: sna8810_0s at: 8/14/2017 2:11:24 PMLast edited by: Jen_Moderator at: 8/14/2017 2:20:29 PMCrossed out the solved problem. Last edited by: sna8810_0s at: 8/15/2017 6:59:38 AMLast edited by: The Helping Hand at: 9/8/2017 1:09:40 PM |
|
| 8/28/2017 11:50 AM | |
|
Posts: 648 Rating:
|
Hello Sna8810, in WinCC it isn't possible to count number of alarms in different classes and groups. With best regards rh1990 |
| 7/10/2024 4:48 PM | |
|
Posts: 3 Rating:
|
Has this function been added in WinCC v8? |
Follow us on