(2)| 1/6/2018 2:38 PM | |
|
Joined: 3/28/2015 Last visit: 12/19/2025 Posts: 727 Rating:
|
Hello, Perhaps the following topics might help: 1-Which organization blocks do you need for error handling in STEP 7 V5.5? |
|
Eng.Mohamed Ibrahim |
|
This contribution was helpful to
|
|
| 1/6/2018 3:24 PM | |
|
Joined: 9/27/2006 Last visit: 12/25/2025 Posts: 12474 Rating:
|
Hello hamed; To add to the information provided by Online Tech (Moh. Ibrahim), there are dedicated organization blocks (OBs) that are known as "diagnostic OBs". they are used to gather information from the CPU's OS whenever a fault is detected during opertion. The diagnostic OBs are OB 80 to 88, OB 121 and OB 122; see the screenshot below, taken from the System and Standard Functions manual: Chapter 1 of the manual examines the different types of OBs available to structure a Siemens PLC program; you should examine the structure of the local data of each diagnostic OB, for example OB 86 (Rack Failure OB) on page 66. The local data registers are used to gather data from the CPU about a fault, if the error is linked to a lost remote I/O rack (Profibus or Profinet). While this OB is being processed, without any internal programming, the CPU will continue working, even though a fault has been detected, because it is communicating with this OB 86 local data. Once it has gathered the information and placed it in the diagnostic buffer, it will return control to OB1 and continue processing the program instructions. So it will not go to STOP, but the diagnostic LEDs will be activated to indicate there is an intervention required by the programmer. The following discussion provides information on the same subject, it could be interesting to you: https://support.industry.siemens.com/tf/WW/en/posts/problem-on-cpu-315-2dp/90455?page=0&pageSize=10 Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 1/6/2018 3:26:36 PM |
|
This contribution was helpful to
|
|
| 1/8/2018 3:37 PM | |
|
Posts: 241 Rating:
|
great!! exactly i have got my questions answer it is my honor that i can communicate with so high experienced and knowledgeable friends like you in this forum |
Follow us on