6/20/2024 5:31 AM | |
Joined: 4/28/2015 Last visit: 8/6/2024 Posts: 358 Rating: (38) |
Hi As you have mentioned an PC I am assuming you Sinumerik one machine is fitted with an IPC? If this is the case you can remotely view the current display on the HMI using a VNC Viewer application. You may need to open port 5900 in the windows firewall for this to be allowed through. There are a number of VNC Viewer applications available, RealVNC, Ultra VNC etc. Siemens also sell the product Access MyMachine /P2P for PC/PG (based around a WinSCP style application) which allows you to transfer files to the connected system. https://mall.industry.siemens.com/mall/en/WW/Catalog/Product/6FC5860-7YC46-0YA0 Note: this would allow you to reach the machine via your companies internal LAN, you would not be able to remote onto the machine from a location outside of your company network but using either a VPN or a service such as team viewer. Hope this helps Luke |
Last edited by: The Helping Hand at: 06/20/2024 08:22:37Link optimized |
|
Follow us on