4/30/2021 9:25 AM | |
Joined: 1/9/2018 Last visit: 10/24/2024 Posts: 1 Rating: (0) |
Hi, I have another question regarding replacement of 6ES7315-2AF03-0AB0 to 6ES7315-2AH14-0AB0; where i change the HW config plc module only. The system is connected via profibus to control IOs and Drives; the current issue is with the drives after the PLC replacement. Its connected to 4 6SE7090-0XX84-0FF5 (MDW) and 1 6SE7090-0XX84-0FF5 (SG70). The issue is with 6SE7090-0XX84-0FF5 (SG70); where i’m unable to send a run command through communication; everytime i tried to run.. an alarm occurs, and the keypad in a split of ms shows 010 008 then back to 009. As for 6SE7090-0XX84-0FF5 (MDW) runs well Can anyone guide me on solving this problem? Thank you ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/30/2021 10:56:19New subject after splitting |
|
Follow us on