3/8/2023 8:36 AM | |
Joined: 2/22/2023 Last visit: 4/12/2023 Posts: 5 Rating: (0) |
Any posibilities to add a block to TIA portal v16 like a PLC, router, etc. (?) I'd been troubleshooting some error with node-red and Lib-s7 and thought: Mabye is an error with TIA Portal communications? My project is not for educational purposes. I'm using a 1212 DC/DC/DC and a 1212DC/DC/RLY but neither of them can load information in the gateway... :"D Whenever I upload and deploy the node-s7 (Read or Write, none works) the same IP as the plc has it disconnects itself going into a loop of "Lost connection to server, Reconnecting..." I used node red 1.2.1 ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/08/2023 10:43:41New subject after splitting |
|
3/8/2023 9:30 AM | |
Joined: 2/22/2023 Last visit: 4/12/2023 Posts: 5 Rating: (0) |
Hi, I am using the version 3.1.0 with an IOT 2040 6es7 647-0aa00-1ya2 |
3/8/2023 9:37 AM | |
Joined: 4/28/2015 Last visit: 11/11/2024 Posts: 3345 Rating: (379)
|
Hi, you can't use V3.x of the s7 nodes - there is lots of topics here already. See e.g. here. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
Follow us on