1/2/2010 7:31 AM | |
Posts: 6 Rating: (0) |
Hello everyone! In some classes of chicks only need heating for 10 days, then schedule a fixed temperature for the day, something like this. Day 1 = 31.00 ° C Day 2 = 30.75 ° C Day 3 = 30.50 ° C Day 4 = 30.00 ° C Day 5 = 29.75 ° C Day 6 = 29.25 ° C Day 7 = 29.00 ° C Day 8 = 28.5 ° C Day 9 = 28.00 ° C Day 10 = 28.75 ° C the problem comes when heating is needed for 15 days or more, the blocks are not enough! My question is: There any way to get temperature curve for example with maximum and minimum temperature (31.00 - 28.75) and the Logo! Scroll the temperature curve in the 10 days? Is that possible in logo! Thanks. AttachmentTemperature Chicks.zip (525 Downloads) |
Last edited by: tecnoelectron at: 1/2/2010 8:49 PMI''m sorry friends some parameters of the program were wrong. Already corrected and updates. |
|
1/2/2010 11:12 PM | |
Joined: 1/5/2007 Last visit: 4/7/2023 Posts: 1690 Rating: (580)
|
Hi, sorry i have no more time now, so.. ...do you need a curve to use in your circuit, then look at CO2 calculation - Math equations with LOGO! or you can use memories builded by a circuit--look with SEAECH... If you only wont to display all the values with separate time stamps - that is not possible (look answer before) Best regards Betel |
==> Meine TAG-Listen: "deut." |
|
Follow us on