9/19/2024 9:50 AM | |
Joined: 5/30/2024 Last visit: 9/19/2024 Posts: 2 Rating: (0) |
Hi HedeyL, I am working with an S7-1500, model 1517F-3 PN/DP, along with several Unified Comfort panels (MTP700, MTP1200, MTP2200). I am using TIA Portal v19; the firmware of the panels is 19.0.2, and the PLC firmware is 3.1. I am trying to connect each panel to the LSNTP server to synchronize them with the PLC. I have configured a single NTP server on the panels, using the PLC's IP address. However, when I enable the FB-LSNTP block, I encounter error 8601, as shown in the picture below. I am also having trouble finding information on where to locate the connID for the panels. Could you please help me with this? ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 09/19/2024 10:34:59New subject after splitting |
|
Follow us on