3/17/2019 9:04 AM | |
Joined: 10/10/2015 Last visit: 12/20/2023 Posts: 1 Rating: (0) |
Dear collegues, I have an IPC277D with intel Atom 1.0GHz E640, Windows 7 Ultimate x32 now with 1024x768 resolution in 32-bit. I Installed ELO SW for touch screen correctlly, but now I have a problem with settings of resolution to required 1366x... I treid to find LVDS and CRT driver 1.5.2 1812, but I am not able to find it. I installed IMEGD for display controlled extension correctly, but I cannot take a resolution from IPC higher than 1024x768 - it shows to me that standard monitor VGA is ON. Also I disabled standard monitor VGA driver. Have someone correct instalation for graphics driver? Thank You for help.
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 3/18/2019 12:27:02 PMNew subject after splitting |
|
12/17/2019 12:26 AM | |
Posts: 1 Rating: (0) |
Hi, I have the same problem. I download the driver "graphic LVDS and CRT 1.5.2.1816 (for driver function_0)" from: ftp://data.aaeon.com.tw/DOWNLOAD/Drivers/GENE-TC05/Step%202c-%20Graphic%20LVDS%20and%20CRT.exe Manual instalation and Works!!!! 1366x768. This replaces the disabled VGA Standard driver, detect as dual monitor but adjust resolution and reboot!! |
Last edited by: Jimmy A. Vega at: 12/17/2019 00:28:32 |
|
6/13/2020 2:11 PM | |
Posts: 1 Rating: (0) |
Many many many thanks for this info i was fighting with this resolution 3 days. As usual is very simple :D Thanks for this comment. |
Follow us on