1/6/2024 8:05 PM | |
Joined: 12/18/2014 Last visit: 7/16/2024 Posts: 33358 Rating:
|
To do this, I would first have to see your LSC program and the LWE project. Please upload both as a ZIP file. |
1/6/2024 11:45 PM | |
Joined: 1/3/2024 Last visit: 2/18/2024 Posts: 18 Rating:
|
Here is the .lsc file. I believe it is understandable. There are 4 buttons (Inputs) : Push Button (I1) one click ----> load 1 ON/OFF (Q1) Push Button (I1) double click -----> Load 2 ON/OFF (Q2) Same for push buttons 2 & 3 Push button 4 (I4) ------ > one click all Loads ON, Hold for 30ms all loads off The LWE file I deleted since it was not working, but it was the same concept, 4 digital (switch buttons) (I1 to I4) (as I1, I2,I3,I4) and 6 digital outputs Q (Q1 to Q6) Thank you Attachmentlsc.zip (212 Downloads) |
1/7/2024 3:54 AM | |
Joined: 12/18/2014 Last visit: 7/16/2024 Posts: 33358 Rating:
|
I created something for you so that you can see how you can switch via the web server. The way you built your circuit doesn't work properly. The double click is not recognized; you can only switch the first output. This is because the network creates delays. AttachmentPikermi-Khpos.zip (190 Downloads) |
1/7/2024 12:14 PM | |
Joined: 12/18/2014 Last visit: 7/16/2024 Posts: 33358 Rating:
|
I can't say anything about other platforms such as KNX, etc.. The LWE V1.2.0 is part of the upgrade package to LSC V8.4. Download and installation instructions for LOGO! Soft Comfort Upgrade V8.4 |
1/7/2024 7:37 PM | |
Joined: 1/3/2024 Last visit: 2/18/2024 Posts: 18 Rating:
|
Thank you I downloaded LWE V1.2.0 and I did some modifications in .lsc file as well based on your example by using Network Inputs (Flags are not working for me). Everything works nice. The physical (real) push Buttons works perfect (one & double click, along with one click and hold for 30ms as well) The control through LWE is modified (since double click and other functions are not supported) but it is a graphic environment so there is no big problem. Thus, I made 2 buttons for each work. Just for your info and for everyone is interested or have similar project I upload both the .lsc file and the LWE files (graphics need some improvement by the way). * You will see the additional network inputs with red color. Thanks again for all the help George P.S. : It it a bit weird to have your program completed and if you need (or the client need) to upload it in LWE then you have to make modifications by adding Network Inputs and "OR" Blocks etc. Maybe software engineers need to address somehow some matters. AttachmentLWE_&_LSC.zip (248 Downloads) |
Follow us on