7/12/2024 12:19 PM | |
Joined: 2/15/2021 Last visit: 10/8/2024 Posts: 12 Rating: (0) |
Hello everyone, I am working on an IOT2050 Advanced (6ES7 647-0BA00-1YA2) / FS:05 with firmware version 2022.01-V01.03.01.01-0-gffc3caf. I just installed the SD card using the example image: 109741799_RT_IOT2050_Example_Image_RT_V1.3.1_PNDriver_2.3.zip. As a result, I have Node-RED version v2.2.2 and Node.js version v12.22.12. The system functions perfectly with all the development we have done. However, we are encountering a significant issue when serving data via OPC UA. Node-RED crashes every time I add an OpcUa-Server node from the node-red-contrib-opcua library 0.2.262. I have tested several examples found on this forum and other websites, but the behavior remains the same: Node-RED crashes. Any help or suggestions to resolve this issue would be greatly appreciated. BR AttachmentJournal Jul 12 115031 iot2050-debian node-r.txt (172 Downloads) |
9/24/2024 12:58 PM | |
Joined: 4/3/2020 Last visit: 9/30/2024 Posts: 23 Rating: (0) |
But how to fix it? Which xml? |
Follow us on