5/9/2013 12:28 AM | |||
Joined: 9/27/2006 Last visit: 9/4/2024 Posts: 12282 Rating: (2682) |
Hello syd; The unit you have is basically a PC, not a PLC. (and the part number is 6AV7 812-1AC23-0AA0). Open this link top the Technical Data for that Industrial PC unit: http://support.automation.siemens.com/WW/view/en/28485442/td You can see it has a Windows OS and other features of a PC. If you really want to, you can load a SoftPLC such as WinAC RTX to run it as a PLC, and run a Step 7 PLC program controlling remote Profibus-DP IOs. See this link for more information:
Daniel Chartier |
||
Follow us on