5/9/2022 7:24 PM | |
Joined: 10/17/2007 Last visit: 9/4/2024 Posts: 4012 Rating: (353)
|
Hi, jflopezven,1st of all can you let me know which country are you working now? I checked your all posts, you seem to have some old Siemens SIMODRIVE back to 1980''s such SIMODRIVE 610 and SIMODRIVE 650 series. both of them discontinued for more than 20 years. I myself worked in 1990 in the Siemens Factory in Germany the factory made those drives, as a final inspector. I really watched them the last years of life--At that time Siemens new generation of SIMODRIVE 611 --1st modular servo drive system in Siemens Motion Control , which combinates--#1 Power Supply module;#2 Feed servo drive module;#3 Spindle Drive module; #4 other related modules . For you question today is about SIMODRIVE 650 series, it is an old spindle drive. I really did some service cases from 1990 to 1993, but how many years? forget everything. But I can give you some suggestion, may out of technical scope but hope can help you. #1-- Replace your old 650 with SIMODRIVE 611A system , only use its spindle module I attached motor cade list, there is no 1PH6161-4CF00- but there is 1PH6161-4NF00, for detail you can PM me if you accept this suggestion #2--If you wan to keep your old system, suggest go to online market such as eBay to look those 2 cards , order them one at the time to see if it helps. #3--If #2 not help, you can only to call you local electrical repair shop try to fix the cards Hope it helps
Attachment611A_SP_Motor_Module_Code.pdf (773 Downloads) |
Last edited by: nulizhang at: 05/09/2022 19:25:32If you like my comments please |
|
5/10/2022 1:06 AM | |
Joined: 9/5/2016 Last visit: 7/16/2024 Posts: 11 Rating: (0) |
Hello, and thank you for answering. I am in Colombia, but previously I worked in Venezuela. I have been working many years with the Siemens Sinumerik line specially the 810T/M, 810D/840D Power Line series and to this day I do retrofit services on the 808D/828D series. To be competitive with our prices and services we try to keep as many original parts as possible from each machine, particularly the motors and drivers of the spindle in this case. I comprehend that there are discontinued machinery and devices, but it’s Siemens reliability, stability and quality allows us to keep using them in the retrofit of CNC (Lathe/Mill) machinery. In some cases the retrofit is so effective that machines work for years and years without any sign of issues, in this specific case is the driver installed in a Gildemaister CTX400 lathe. I attached the drivers manual and fault codes of the Simodrive 650 driver. The issue does not lay on the 611 Simodrive (6SN1145) and its motor modules (6SN1123). Thank you for your interest, and I hope that you can help me solve this issue. Jflopez Attachmentsimodrive 650 errors.pdf (631 Downloads) |
5/10/2022 1:11 AM | |
Joined: 9/5/2016 Last visit: 7/16/2024 Posts: 11 Rating: (0) |
Manual is too large to upload it here. http://support.automation.siemens.com/WW/view/en/21914234 |
5/11/2022 1:27 PM | |
Joined: 10/17/2007 Last visit: 9/4/2024 Posts: 4012 Rating: (353)
|
I suggest you do my suggestion #2, see my attached file including 2 links. The supplier is in USA one of big and relative reliable used Siemens parts. I myself also use them for my customer You can order 1st one and try feedback please
Attachment650_parts.docx (753 Downloads) |
If you like my comments please |
|
Follow us on