7/16/2024 10:47 AM | |
Joined: 5/6/2022 Last visit: 7/22/2024 Posts: 432 Rating:
|
Hi AutoGen_1583874, Was something changed in the Java file during installation? Where did you get the software from, directly from SIOS, from software you received or from third parties? You also need full administrator rights for installation and use. Also tell you, does this happen to you with any project you try to create? Best regards!
|
If this Information really helps, you could use the Rate function |
|
7/16/2024 9:29 PM | |
Joined: 7/15/2024 Last visit: 7/16/2024 Posts: 2 Rating:
|
I do not think anything was changed in the Java file during the installation. The upgrade to 8.4 came from SIOS. I do have full rights. It happens with any new or existing projects. The existing projects can be opened and loaded onto a new device using 8.4 but the error pops up when I try to select the hardware or set the clock on LSM. |
Follow us on