12/13/2010 6:00 PM | |
Posts: 10 Rating:
|
I am using MP377 to storage the trending data in CF card. I would like to know that can I use 8G or aboveCF card in MP377 as storage media. Regards, Creater |
12/14/2010 8:59 AM | |
Joined: 4/24/2006 Last visit: 9/15/2025 Posts: 9027 Rating:
|
Dear Creater, Have a look at this link: Which external storage media can you use with the SIMATIC panels and which memory card interfaces do they have? In link you can download PDF, here you see maximum size of card. Best regards, Wizard |
12/14/2010 9:25 AM | |
Joined: 4/29/2010 Last visit: 1/20/2025 Posts: 1557 Rating:
|
Hello, i don`t know if this will work but look at this FAQ, there you can find the information that the MP377 supports max. a 2GB storage device: Which external storage media can you use with the SIMATIC panels and which memory card interfaces do they have? Best regards. |
12/14/2010 1:21 PM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
The max. capacity which is tested officially is 2GB, (already mentioned above). Best regards, Hristo Mihalev |
Follow us on