6/29/2023 8:06 AM | |||||||||
Joined: 5/5/2020 Last visit: 7/11/2024 Posts: 40 Rating:
|
Dear Experts, I have TIA V17 Update 6 , i am tried to import project from TIA Selection Tool but i got the error message : The module with the MLFB '6ES7 515-2AN03-0AB0' is not available in this TIA Portal installation. (as shown in the attached picture) . i installed update 6 and also i installed the following hardware support packages : Support Packages for TIA Portal V17
all the above hardware support packages were installed but the CPU : '6ES7 515-2AN03-0AB0' still doesnot appear . Please can you help me how can i add the S7 1500 CPUs to TIA v17 ? . Best Regards |
||||||||
2/9/2024 7:29 PM | |||
Joined: 8/10/2023 Last visit: 9/3/2025 Posts: 2 Rating:
|
Hello Maybe are you know 6ES7511-1FL03-0AB0 (S7-1511F 1PN 450kb/1.5mb) has same situation? Thanks |
||
2/10/2024 9:31 AM | |
Joined: 3/30/2020 Last visit: 9/12/2025 Posts: 5446 Rating:
|
Best to use the search facility available on this web page Than you will find the answer.. (bottom of the picture)
|
Last edited by: qwazee at: 02/10/2024 09:33:52Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
This contribution was helpful to
2 thankful Users |
11/22/2024 11:28 AM | |
Joined: 2/19/2024 Last visit: 11/22/2024 Posts: 1 Rating:
|
HELLO HOW TO ADD CPU S-1500 6es7511-1fL03-0ab0 IN CATALOGUE HARDWARE TIA V17 |
Last edited by: aziz_grb172 at: 11/22/2024 11:36:27 |
|
11/22/2024 11:43 AM | |
Joined: 3/30/2020 Last visit: 9/12/2025 Posts: 5446 Rating:
|
YOU CANNOT ADD THE CPU. YOU HAVE TO USE ANOTHER ONE. THIS ANSWER WAS ALREADY GIVEN ONE REPLY YOUR QUESTION. PHONE A SIEMENS OFFICE IF YOU DOUBT THE ANSWER. |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
12/22/2024 3:57 PM | |
Joined: 4/6/2021 Last visit: 5/29/2025 Posts: 2 Rating:
|
So, basically you load the hardware configuration program with the old CPU 1FK0x and th new 1FL03 will load it without errors or there is a specific procedure to do so? thanks in advance and Happy Holydays to everyone, Mike |
12/22/2024 8:23 PM | |
Joined: 9/21/2012 Last visit: 9/10/2025 Posts: 4708 Rating:
|
You just download it, it will give a message to you that there is a difference in the online/offline part number, but you can still download the it will function normally. |
This contribution was helpful to
1 thankful Users |
Follow us on