7/9/2010 11:45 AM | |||||
Posts: 81 Rating:
|
Hello,
Thanks for your previous help ,in existing system of S5 we have CP 143(6GK1143-0AA01) and on PC side we have CP1413 so still I can use CP 1613 A2 in replacment of CP1413 can we use any of these models of CP 1613 in replacemnet of CP1413 From the Siemens A&D Mall:
|
||||
Last edited by: O_Moderator at: 7/9/2010 12:04 PM |
|||||
7/9/2010 12:16 PM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
Hello, Yes, you could. I suggest you to contact with Siemens offices in your place. Look at Change Over from CP 1413 to CP 1613 .Take in mind 3 points: 1. The user interfaces of the software products based on the CP 1613 are compatible with the correspodingBest regards, Hristo Mihalev |
5/21/2015 7:05 AM | |
Joined: 5/26/2011 Last visit: 9/10/2025 Posts: 482 Rating:
|
Hello sir UMENCHO, The link on your post is not working, could you give me a new one? So you're saying that for instance, I can replace the CP1413 of my WinCC station that is communicating to S5 CPUs by CP1613 without any problems right? Maybe I just have to do some settings on the PC driver as well as WinCC tag management? What about on the S5 side, would there be other changes required for this? What if I replace an old WinCCv4 station running on Windows NT using CP1413 to communicate with S5 CP1430TF with a new PC station, say WinCCv7 running on Windows XP using CP1613? Can you specify all the software/configuration changes that should also be done with this hardware replacement? Maybe you can also help me on this related inquiries: https://support.industry.siemens.com/tf/ww/en/posts/backup-wincc-for-an-old-s5-wincc-system/126908/?page=0&pageSize=10 Thank you very much for any response! |
Last edited by: G_R_E_Y at: 5/21/2015 7:55:43 AM |
|
Follow us on