7/9/2017 9:50 AM | |
Joined: 1/11/2015 Last visit: 6/8/2023 Posts: 32 Rating:
|
Hi All; I'm using Analoge card 6ES7331-7KF02-0AB0 in my project I have 6 2-Wire 4-20ma Transmitters, I would like to know if my connection is correct because I heard that only the first 4 channels work with 2-wire 4-20ma transmitters my connection: Transmitter 1: CH1 (+) Terminal with Terminal (2) on the Card (-) Terminal with Terminal (3) on the Card Transmitter 2: CH2 (+) Terminal with Terminal (4) on the Card (-) Terminal with Terminal (5) on the Card Transmitter 3: CH3 (+) Terminal with Terminal (6) on the Card (-) Terminal with Terminal (7) on the Card Transmitter 4: CH4 (+) Terminal with Terminal (8) on the Card (-) Terminal with Terminal (9) on the Card Transmitter 5: CH5 (+) Terminal with Terminal (12) on the Card (-) Terminal with Terminal (13) on the Card Transmitter 6: CH6 (+) Terminal with Terminal (14) on the Card (-) Terminal with Terminal (15) on the Card for the schematic wiring diagram its in the attachments so, I would like to know if I can use 2-wire 4-20ma in the 8 channels or only in the first 4 channels AttachmentLoop diagram Model (1).pdf (835 Downloads) |
7/9/2017 10:50 AM | |
Joined: 5/6/2010 Last visit: 8/31/2025 Posts: 2029 Rating:
|
Hello, you can use all 8 channels with 4...20 mA transmitter. This folow things are important:
I hope this is helpful for you. regards |
This contribution was helpful to
1 thankful Users |
7/9/2017 3:02 PM | |
Joined: 1/11/2015 Last visit: 6/8/2023 Posts: 32 Rating:
|
Thank you very much; can I just connect 10 and 11 to 20 ?? |
Follow us on