5/31/2008 2:47 PM | |
Posts: 115 Rating:
|
Dear Experts, Let's I explain the problem, in PCS7 V7.0+SP1 , I implement my project with cross network projects and I have 7 Project,(5 pump station,1 Main Station,1 Monitoring Station)in each pump station I have one AS-H and 2 single station (OS) and the hierarchy level started with the level 2 of OS for proper monitoring of the Pump Stations, in the monitoring project I have 2 redundant server and some client and I made the Update in Multiproject and make the copy of hierarchy folders of other projects in monitoring project. But I can't put the level of hierarchy of OS in monitoring project to 1 because apparently the Hierarchy level of all projects should be same, and I need to put the Monitoring project to Hierarchy level 1 in OS Area to proper monitoring the pump station with their sub folders, I don't have a problem with the OS in Pump stations I just want to put the hierarchy level of the OS in Server in Monitoring station to 1, I put the Hierarchy level of the plant in the attach in 2 view. Is this possible and what should I watch out for doing this? Thanks in Advance, Saeed AttachmentDesktop.zip (436 Downloads) |
Follow us on