2/4/2025 3:51 PM | |
Joined: 10/19/2016 Last visit: 7/11/2025 Posts: 316 Rating:
|
Hi, The feedback encoder and the electric motor are both functioning correctly but not communicating properly in Sinumerik ONE CNC. Here the link: the first 3 rows increase and then abruptly come back to zero. 2 drive and 2 rotary axis, AX10 and AX11. I know the motor is receiving current and the encoder is reading but it seems that after several JOG+ the system is not moving and returns error. The CNC is controlling an HLA module that will control a third party drive to rotate an axis. What could I check for the correct axis rotation? |
Last edited by: gtsolid at: 02/04/2025 15:52:23Last edited by: gtsolid at: 02/04/2025 15:54:41𓋹 Siemens 840Dsl + TIA v17 𓋹 |
|
Follow us on