6/4/2012 11:41 AM | |
Joined: 12/29/2011 Last visit: 8/31/2025 Posts: 39 Rating:
|
Why don't you try to run these large part programmes from the PCU50 Hard disc. There is a Vertical softkey in the menus labelled "Execute fr. hard disk" This function runs your part programme from the hard disc, automatically transmitting into the nc sections of the part programme as needed. Your part programme size will then only be limited by the Hard Disc, Attached is the section from the Operators Manual which explains how to do this. Best Regards Mr_Al AttachmentExecution_from_HD.pdf (190 Downloads) |
6/25/2012 6:27 AM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
Hello Steve, Thanks, it works. DEEP. |
Follow us on