7/26/2009 7:04 PM | |
Posts: 1 Rating:
|
Hi, I've been having a problem when it comes to compiling my OS project. Until recently the OS has been compiling without error, now though, i get an internal error 10006 and the compiler complains about synchronizing data with an 'AND' block that was recently added to a chart within the AS program. I've tried taking the AND block out, taking the whole CFC chart out, re-organising the project etc but it still complains about an internal error (however, it seems to be a general error rather than relating to a specific AND block). I've attached some screen dumps of the original error. Thanks in advance, Neil AttachmentS108225julyError.zip (131 Downloads) |
Last edited by: neilmac at: 7/26/2009 9:18 PMLast edited by: neilmac at: 7/26/2009 7:05 PM |
|
7/27/2009 10:02 PM | |
Posts: 2661 Rating:
|
Do you get the error 1739:10 when you save-as with reorganization? see if the following is applicable in your case: What can you do to avoid the message "Invalid file position" (1739:10) when saving your project with "Save as ..." and the option "Reorganization (slow)"? |
Follow us on