8/1/2013 7:09 AM | |
Posts: 29 Rating:
|
Good day below i system architecture of my system and i have some clarification please answer and verify accordiingly ( please see attach file ) 1. Is this system already a profisafe system? 2. please add item needs for this system to be fully SIL certified 3. How to achieve and convert standard profibus to profisafe? 4. do i need safety separator in my et200? ( in the diagram i did not include separator) 5. S7 400 racks include CP 441-1 beside CPU, is this also a SIL certified??? i need 441 for ASCII protocol. if not SIL please suggest other item that will comply and satisfy my needs 6. this system is for oil and gas application 7. please show me the right system architecture if this is not right AttachmentPresentation1.zip (435 Downloads) |
Last edited by: exponent at: 8/1/2013 7:12 AM |
|
8/3/2013 2:09 PM | |
Joined: 7/2/2008 Last visit: 8/7/2025 Posts: 928 Rating:
|
Helloexponent, Hello David, Thank you David for your excellent post. I just have two small comments.
The integrated Profinet ports of the V6 CPUs support fault tolerant connection through ISO on TCP. It can be used instead of theCP443-1.
This was mandatory before SIMATIC NET V8.2. Now the REDCONNECT can be softnet by using the newSIMATIC NET SOFTNET-IE S7 VM REDCONNECT V8.2. So, For small systems you don't need the CP1623 anymore. Best regards, H-H |
This contribution was helpful to
1 thankful Users |
Follow us on