2/13/2023 3:50 PM | |
Joined: 2/17/2020 Last visit: 9/11/2025 Posts: 1251 Rating:
|
Hi again, If you can't even ping the HMI... I recommend you try the Reset option via USB, following this FAQ: USB Recovery (Reset to factory) Mode for 2nd Generation Basic Panels If it is also not possible to update the OS later this way, or to ping the panel, maybe it should be sent in for repair! |
A rating will be well appreciated. |
|
2/14/2023 9:06 AM | |
Joined: 8/7/2019 Last visit: 6/30/2025 Posts: 4 Rating:
|
Hi! Thank you for answer. Problem is that our panel KTP600 PN does not have USB port, only ETH/PN. Thank you, |
3/15/2023 2:24 PM | |
Joined: 8/3/2009 Last visit: 9/16/2025 Posts: 16434 Rating:
|
Hello Byrpierce It should be possible to work with prosave and the MAC address of the device to do a reset to factory settings. Check in the Manual: https://support.industry.siemens.com/cs/de/en/view/31032678/27914322699 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on