(2)| 7/1/2009 7:15 AM | |
|
Joined: 10/7/2005 Last visit: 1/16/2026 Posts: 3054 Rating:
|
Hallo Ninja Robot have look at this thread (and especially H-H's advise). HMI connect to Redundant PCL S7-313-2DP using SW redundancy |
|
Cheers |
|
| 7/1/2009 7:35 AM | |
|
Posts: 691 Rating:
|
Hello Fritz The manual which I got describes coneection in WinCC and other Third party communication But I want to make "connection" in WinCC Flexible |
| 7/1/2009 8:42 AM | |
|
Joined: 7/2/2008 Last visit: 12/21/2025 Posts: 929 Rating:
|
Hello Ninja Robot, In the thread which Fritz has given, you would find a link for FAQ posted by JMJ. In this FAQ take another look atexample No. 5 where you will read In Entry ID: 23842653 you will find a function description and a sample project in which this functionality is implemented. Read this entry carefully and you can just usethe same concept for creating connection for software redundancy. It's typically the same. Also check this thread. You can use scripts to change connectionand I think it should also work. Best regards. H-H |
This contribution was helpful to
|
|
| 7/1/2009 9:58 AM | |
|
Joined: 5/8/2006 Last visit: 10/23/2025 Posts: 1085 Rating:
|
Hi Maybe this faq will help you: http://support.automation.siemens.com/WW/view/en/22584323 Ethernet connection is similar. Bye |
| 7/29/2009 11:35 AM | |
|
Posts: 382 Rating:
|
Dear Ninija Robot, 1] The link given by H-H is quite clear. |
Follow us on